2017-03-28 7:31 AM
Is it possible to connect an external eeprom to the SPWF01.21 module? The stored eeprom data will be very small >1K and only serve to remember GPIO high or low settings of the modules STM32F103 core that an end user will periodically set if the module loses power. Which interface? I2C, SPI, GPIO, Serial?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.