2011-10-21 1:54 AM
Spruce -SolidDigi STM32 ARM cortex board can be used with
http://www.cutedigi.com/product_info.php?products_id=4408
and is compatible withhttp://www.cutedigi.com/product_info.php?products_id=4407
.It can be used in GCC+Eclipse+openocd+openJtag and Arduino enviroment!
Spruce has Arduino compatible shield pins, all the Arduino shields can be used on SolidDigi STM32 cortex board. Arduino similar IDE can be used to download Arduino code to Spruce board.
Spruce Hardware Resources:
Arduino IDE Enviroment
In Arduino IDE enviroment, it is fully compatible with maple, and all arduino shield. The bootloader is flashed through RS232 port, and the arduino program is downloaded frm USB port. The driver of the USB port can be found at the maple IDE, which can be downloaded from:
http://www.soliddigi.com/pub/SOLID_STM32/Tools/Solid-ide-0.0.11-windowsxp32.7z
Download:
GCC+Eclipse+OpenOCD+OpenJTAG
Spruce also supports development using GCC+Eclipse+OpenOCD+OpenJTAG.
Download:
http://www.soliddigi.com/download/showdownload.php?id=50&lang=en
:http://www.soliddigi.com/download/showdownload.php?id=50&lang=en
2011-10-24 6:26 AM
I'd stay miles away
how much would you trust a company that shamelessly hijack a discussion forum to peddle their stuff. ErikWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.