2020-06-17 12:36 PM
Hi guys,
Probably the question has been asked one million times but being new on this site, i did not find any clue. My problem is using STM32F446 on SPI1 with DMA2 addressing a device (ADIS16488) in 16bits SPI in mode 3. Polling works perfectly but seems a little time consuming for me. I tried the IT and DMA but I am facing a problem I cannot solve. When I want to perform a transfer in burst , let s say a 12x6bits array, in IT and DMA only a transfer only one halfword it succeeds, if more that one halfword, the second data on MISO is 0x0000. I think that my slave can not take the burst mode (stall time between data is 2µs min) and the second 16bits command is lost so I was wondering if there is a way to insert a little pause in the sck signal between two consecutive halfwords transfers in order to respect those 2µs.
I thank you for your help
olie
Solved! Go to Solution.
2020-06-17 1:16 PM
Run TIM1 or TIM8 with a period of the 16-bit frame plus the delay. Use that timer to trigger DMA feeding the SPI Tx. Leave SPI Rx as it is now.
JW
2020-06-17 1:16 PM
Run TIM1 or TIM8 with a period of the 16-bit frame plus the delay. Use that timer to trigger DMA feeding the SPI Tx. Leave SPI Rx as it is now.
JW
2020-06-17 1:20 PM
Thanks Jan,
That's an interesting idea.
Olie
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.