STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SPI full duplex mode 3 using DMA.

Hi guys,Probably the question has been asked one million times but being new on this site, i did not find any clue. My problem is using STM32F446 on SPI1 with DMA2 addressing a device (ADIS16488) in 16bits SPI in mode 3. Polling works perfectly but s...

papageno by Associate III
  • 1756 Views
  • 2 replies
  • 0 kudos

Resolved! What are the voltage levels for RCC_OSC_IN

I want to use a HSE BYPASS Clock Source configuration with an stm32f301k6t.Unfortunately I could not find any information in which voltage range my external oscillator should operate. Sorry if the answer is trivial, I'm no expert in electrical engine...

fal.sch by Associate II
  • 1811 Views
  • 2 replies
  • 0 kudos

STM32F7 chip option bytes corruption

Overview : In my project, I use two ST controllers which communicate over UART. 1st controller ( A ) has an intelligence to upgrade firmware of 2nd controller ( B ). This upgrade happens by initiating bootloader over UART of B by A. ( Boot 0 pin is u...

svLag by Associate II
  • 821 Views
  • 0 replies
  • 1 kudos

Fixed-wing UAV flight controller design

Hello everyone, I am a PhD student in the field of autonomous guidance of small UAVs.I have done the design of the flight controller for small fixed wing UAV and evaluated it through HIL and comparing the simulation results with the HIL results.Now I...

SPI/DMA Setup for Burst SPI reads

Posted on November 06, 2017 at 10:37HelloI am interfacing the STM32F407 with the ADE9000 chip that supports burst reads which means, after requesting a data set (write command from STM32F4) I can clock out as many bytes I can, the chip increments th...

STM32L476RG Nucleo Board

I was wondering if i were able to put 3.8V on the E5V power line. I checked in the User Manual and there is standing this at page 21: E5V CN7 pin 6 4.75 V to 5.25 V 500 mAWhen i look at the datasheet of the step down converter (LD39050):https://www.s...

Fde W.1 by Associate II
  • 3968 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.