2018-03-01 4:28 AM
HI,
i have writing data to DR register
after that in DR register shows 0xFF
addr=0x000080;
addrHigh1 = ((addr & 0xFFFFFF)>>16); addrHigh2 = ((addr & 0xFFFFFF )>>8); addrHigh3 = (addr & 0xFFFFFF); wrenInstruction = WREN; buffer1[0] =WRITE; buffer1[1]=addrHigh1; buffer1[2]=addrHigh2; buffer1[3]=addrHigh3;HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);
HAL_Delay(5); if(HAL_SPI_Transmit(&hspi1, &wrenInstruction,sizeof(wrenInstruction) , 10) != HAL_OK){ } HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET); HAL_Delay(5); HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET); if(HAL_SPI_Transmit(&hspi1, buffer1, sizeof(buffer1), 10) != HAL_OK){ } HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4,GPIO_PIN_SET); HAL_Delay(5); if(HAL_SPI_Transmit(&hspi1, buffer2, sizeof(buffer2)-1, 10) != HAL_OK){ } buffer1[0] =READ; buffer1[1]=addrHigh1; buffer1[2]=addrHigh2; buffer1[3]=addrHigh3; HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET); HAL_Delay(5); if(HAL_SPI_Transmit(&hspi1, buffer1, sizeof(buffer1), 10) != HAL_OK){ } HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4,GPIO_PIN_SET); HAL_Delay(5); if(HAL_SPI_Receive(&hspi1,buffer2,sizeof(buffer2),100)){ } /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE *//* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */}
/* SPI1 init function */
static void MX_SPI1_Init(void){/* SPI1 parameter configuration*/
hspi1.Instance = SPI1; hspi1.Init.Mode = SPI_MODE_MASTER; hspi1.Init.Direction = SPI_DIRECTION_2LINES; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init.CLKPhase = SPI_PHASE_1EDGE; hspi1.Init.NSS = SPI_NSS_SOFT; hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLE; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi1.Init.CRCPolynomial = 7; if (HAL_SPI_Init(&hspi1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
I have configure SPI as FULL_DUPLEX_MASTER in stm32L0 with EEPROM
i have writing data to DR register
after that in DR register shows 0xFF
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.