2023-12-11 6:49 AM
Hello.
I am trying to learn about DMA with spi. I tried HAL library which worked fine for me, I tried the LL Examples (stm32L4x) provided in repository which worked fine when i am reading once with loopback. Now i am trying to use a full duplex master spi with transmit via polling and receive via dma. But i am stuck with how to set the receiving part continously ( in a while(1) loop after rx complete callback) with normal mode as i have to set different address each time i am receiving data from an external chip.
Can anyone provide with some suggestion for this?
2023-12-11 7:23 AM
Hello @prsh
Have you tried SPI_TwoBoards_FullDuplex_DMA example using circular mode? It should help to ensure continuous transfers.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-11 7:44 PM
Yes tried that but my application needs normal mode only to set receive dma before every data receive.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.