2016-12-20 10:20 AM
Hi,
I'm working on 3-Wire(PF7-CLK,PF9-MOSI,PF8-MISO) SPI (SPI5, slave mode, direct mode) using a STM32F769-EVAL.
My goal is to transmit data from SDRAM buffer thru SPI to SPI-Master
I'm using 'HAL_SPI_Transmit_DMA' function to test the above operation.
Here is my problem to setup the SPI DMA.
If It uses the inside SRAM(0x20000xxx) to transmit buffer, It is working fine.
But if It uses the SDRAM(0xC0000000) to transmit buffer, I get DMA FIFO error.
I referred to the example code of CubeMx(STM32Cube_FW_F7_V1.5.0).
it seems like a register setting problem but i can't find what is wrong.
The DMA FIFO error interrupt occurs immediately when HAL_SPI_Transmit_DMA performed.
Code:1) DMA2 FIFO Error pBuf = (uint8_t *)SDRAM_BANK_ADDR; //0xC0000000 -> SDRAM if(HAL_SPI_Transmit_DMA(&hspi5, (uint8_t*)(pBuf), aPacketSz)!= HAL_OK)2) Working Fine
uint8_t dbuf[6144*8]; //0x20000xxx -> SRAM
pBuf = (uint8_t *) dbuf;if(HAL_SPI_Transmit_DMA(&hspi5, (uint8_t*)(pBuf), aPacketSz)!= HAL_OK)
-------------------------------------------------------------------------------------------------------------------------------------------------------------------
static void SPI_Init(void)
{ hspi5.Instance = SPI5; hspi5.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32; hspi5.Init.Direction = SPI_DIRECTION_2LINES; hspi5.Init.CLKPhase = SPI_PHASE_1EDGE; hspi5.Init.CLKPolarity = SPI_POLARITY_LOW; hspi5.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi5.Init.CRCPolynomial = 7; hspi5.Init.DataSize = SPI_DATASIZE_8BIT; hspi5.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi5.Init.NSS = SPI_NSS_SOFT; hspi5.Init.TIMode = SPI_TIMODE_DISABLE; hspi5.Init.Mode = SPI_MODE_SLAVE;if (HAL_SPI_Init(&hspi5) != HAL_OK)
{ Error_Handler(); } }void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi)
{GPIO_InitTypeDef GPIO_InitStruct;
if(hspi->Instance==SPI5) { /* Peripheral clock enable */ __HAL_RCC_GPIOF_CLK_ENABLE(); __HAL_RCC_SPI5_CLK_ENABLE(); __HAL_RCC_DMA2_CLK_ENABLE(); /**SPI5 GPIO Configuration PF7 ------> SPI5_SCK PF9 ------> SPI5_MOSI PF8 ------> SPI5_MISO */ GPIO_InitStruct.Pin = GPIO_PIN_7; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF5_SPI5; HAL_GPIO_Init(GPIOF, &GPIO_InitStruct); GPIO_InitStruct.Pin = GPIO_PIN_9|GPIO_PIN_8; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF5_SPI5; HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);/* Peripheral DMA init*/
hdma_spi5_tx.Instance = DMA2_Stream4;
hdma_spi5_tx.Init.Channel = DMA_CHANNEL_2; hdma_spi5_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE; hdma_spi5_tx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL; hdma_spi5_tx.Init.MemBurst = DMA_MBURST_INC4; hdma_spi5_tx.Init.PeriphBurst = DMA_PBURST_INC4; hdma_spi5_tx.Init.Direction = DMA_MEMORY_TO_PERIPH; hdma_spi5_tx.Init.PeriphInc = DMA_PINC_DISABLE; hdma_spi5_tx.Init.MemInc = DMA_MINC_ENABLE; hdma_spi5_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE; hdma_spi5_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE; hdma_spi5_tx.Init.Mode = DMA_NORMAL; hdma_spi5_tx.Init.Priority = DMA_PRIORITY_LOW; if (HAL_DMA_Init(&hdma_spi5_tx) != HAL_OK) { Error_Handler(); } __HAL_LINKDMA(hspi,hdmatx,hdma_spi5_tx);/* Configure the DMA handler for Transmission process */
hdma_spi5_rx.Instance = DMA2_Stream3; hdma_spi5_rx.Init.Channel = DMA_CHANNEL_2; hdma_spi5_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE; hdma_spi5_rx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL; hdma_spi5_rx.Init.MemBurst = DMA_MBURST_INC4; hdma_spi5_rx.Init.PeriphBurst = DMA_PBURST_INC4; hdma_spi5_rx.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_spi5_rx.Init.PeriphInc = DMA_PINC_DISABLE; hdma_spi5_rx.Init.MemInc = DMA_MINC_ENABLE; hdma_spi5_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE; hdma_spi5_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE; hdma_spi5_rx.Init.Mode = DMA_NORMAL; hdma_spi5_rx.Init.Priority = DMA_PRIORITY_HIGH; if (HAL_DMA_Init(&hdma_spi5_rx) != HAL_OK) { Error_Handler(); } __HAL_LINKDMA(hspi,hdmarx,hdma_spi5_rx); // tx /* DMA2_Stream4_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA2_Stream4_IRQn, 0, 1); HAL_NVIC_EnableIRQ(DMA2_Stream4_IRQn);// rx
/* DMA2_Stream3_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA2_Stream3_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA2_Stream3_IRQn);// spi
HAL_NVIC_SetPriority(SPI5_IRQn, 0, 1); HAL_NVIC_EnableIRQ(SPI5_IRQn); }}void DMA2_Stream3_IRQHandler(void)
{ HAL_DMA_IRQHandler(hspi5.hdmarx);}
void DMA2_Stream4_IRQHandler(void)
{ HAL_DMA_IRQHandler(hspi5.hdmatx);}void SPI5_IRQHandler(void)
{ HAL_SPI_IRQHandler(&hspi5);}2016-12-20 4:23 PM
And can you write into the SDRAM or read from it directly?
JW
2016-12-20 4:49 PM
Yes , The SDRAM is working fine.
I referred to the example code at 'FMC/FMC_SDRAM' on
CubeMx(STM32Cube_FW_F7_V1.5.0).
I can read and write on the IAR IDE.
Thanks,
YC
2017-01-04 6:42 PM
I solved the problem as below.
But I don't know if this is the right thing to do.
void DMA2_Stream4_IRQHandler(void)
{hspi5.hdmatx->Instance->FCR &= ~DMA_IT_FE;
HAL_DMA_IRQHandler(hspi5.hdmatx);}Please advise for me
Thanks,
YC
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.