2024-07-28 5:06 AM - last edited on 2024-07-28 7:13 AM by STOne-32
Hello ,
I have an issue in STM32u575 IN SPI DMA , Even IF I Tried the Example code (/SPI_FullDuplex_ComDMA_Master)
there is no data received from the other side iam using the aardvark to test it
when check the return of this function
HAL_SPI_GetState(&hspi1);
will be : HAL_SPI_STATE_BUSY_TX
I tried all steps and Do the same in another project every Time I faced this issue even if using the Linked - list mode or stander request mode
I receive the same issue with no data may please support in this point ?
Solved! Go to Solution.
2024-07-29 6:35 AM
> SO please Advice what can I do ?
Run the code in debug mode, wait a few seconds, hit pause, see where execution is at.
2024-07-28 11:08 AM
Most of the examples work without issue. If you run the example without changing anything, where does the code end up? Do the LEDs toggle as expected? There are two STM32u575 boards, are you using the correct example? Be detailed.
2024-07-29 12:39 AM
Hello ,
Thank you for your replay
The example code doesn't send any data to the slave when put this line in example
HAL_SPI_StateTypeDef test = HAL_SPI_GetState(&hspi1);
To check the status it is stuck in HAL_SPI_STATE_BUSY_TX , I don't know why each time stuck on it even if the I2c is working with DMA as Example but SPI Not . SO please Advice what can I do ?
2024-07-29 6:35 AM
> SO please Advice what can I do ?
Run the code in debug mode, wait a few seconds, hit pause, see where execution is at.
2024-07-29 10:41 AM
2024-07-30 2:54 AM
Hello ,
Finally the example code is working fine but when trying the same steps in my project the function
HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi)
doesn't call any more it means data stuck and never translate may set some points to check maybe Couse this issue please ?
2024-07-30 3:13 AM
Hello Again ,
Thank you for Your effort I found the issue in software as priority issue there is a lot of tasks and so on that make interrupt does not come so I will solve my project thank you for that
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.