2019-02-18 10:57 AM
Hello,
I am trying to get started with gyroscope L3GD20 on discovery board. I had problems with HAL SPI library so I wrote my own. When I try to communicate with gyro I cant get any answer, I try to read WHO_AM_I register but all the time I got answer 255. Sometimes when I play with address I got value 155 for example and that's it.
Can You tell me if there is some mistake in my code? Thanks in advance
void Initialize_MEMS_Onboard();
void InitializeSPIManually();
void ReadFromMEMSManually(uint8_t address);
void SendDataSPIManually(uint8_t dataToSend);
uint8_t counterForReceive = 0;
uint8_t data1;
int
main(int argc, char* argv[])
{
// At this stage the system clock should have already been configured
// at high speed.
HAL_Init();
Initialize_MEMS_Onboard();
// Infinite loop
while (1)
{
// Add your code here.
}
}
#define CTRL_REG1 0x20
#define CTRL_REG3 0x22
#define CTRL_REG5 0x24
#define FIFO_CTRL_REG 0x2E
#define FIFO_START_ADDRESS 0x28
#define WHO_AM_I 0x0F
void Initialize_MEMS_Onboard(){
__SPI5_CLK_ENABLE();
InitializeSPIManually();
__HAL_RCC_GPIOF_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
GPIO_InitTypeDef GPIO_InitStruct;
GPIO_InitStruct.Pin = GPIO_PIN_7 | GPIO_PIN_8 | GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI5;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_1,GPIO_PIN_SET);
GPIO_InitStruct.Pin = GPIO_PIN_2 | GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
ReadFromMEMSManually(WHO_AM_I);
}
void ReadFromMEMSManually(uint8_t address){
uint8_t addressToSend = (address<<2) | 0b01;
counterForReceive = 0;
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_1,GPIO_PIN_RESET);
SendDataSPIManually(addressToSend);
SendDataSPIManually(0xff);
while(counterForReceive<2);
counterForReceive = 0;
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_1,GPIO_PIN_SET);
trace_printf("%d \n",data1);
}
void InitializeSPIManually(){
SPI5->CR1 |= SPI_CR1_BR;
SPI5->CR1 |= SPI_CR1_CPOL;
SPI5->CR1 |= SPI_CR1_SSM;
SPI5->CR1 |= SPI_CR1_SSI;
//SPI5->CR2 |= SPI_CR2_TXEIE;
SPI5->CR2 |= SPI_CR2_RXNEIE;
SPI5->CR1 |= SPI_CR1_MSTR;
SPI5->CR1 |= SPI_CR1_SPE;
HAL_NVIC_EnableIRQ(SPI5_IRQn);
HAL_NVIC_SetPriority(SPI5_IRQn, 0x0,0);
}
void SendDataSPIManually(uint8_t dataToSend){
while((SPI5->SR & SPI_SR_TXE) == 0 );
SPI5->DR = dataToSend;
}
void SPI5_IRQHandler(void){
if(SPI5->SR & SPI_SR_RXNE){
//receive data here
data1 = SPI5->DR;
counterForReceive++;
}
if(SPI5->SR & SPI_SR_TXE){
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.