2017-07-27 8:31 PM
Hi I'm working on STM32L476RG board when I'm using SPI Peripheral as Receive only mode .In this when im receiving 4 channels data SPI is generating 5 times clock instead of generating 4 times clock.What is the reason for that.
2017-07-28 12:55 AM
Try to use the normal SPI mode (4 wire) where the MOSI signal die in the chip (no GPIO).
Then check if by properly writing on the data register in 4 bit mode (make sure you do a BYTE write access to the DR) to see what happens. Did not experiment on SPI beyond the 8 and 16 bit mode, just guessing.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.