2026-03-20 12:05 AM
I am working on a custom board with STM32F103CBT6TR. Initially, flashing the code resulted in a Hard Fault error, but now it consistently enters a SIGTRAP even after removing all breakpoints. Additionally, the GPIO pins are not toggling as expected. The code is attached as notepad file for reference. Can someone give a solution to this, thank you.
2026-03-20 2:01 AM
Well, I have removed every breakpoint like cleared that used to be present in breakpoint section, but now in debug why it kind of stops in HAL_Delay like it goes to toggle command and then the delay but after that if i resume it just goes out of program like shows this in debug
2026-03-20 3:16 AM
@suba512 wrote:I am working on a custom board with STM32F103CBT6TR.
Please give full details of this board - see:
How to write your question to maximize your chances to find a solution
If it's a Blue (or other coloured) Pill board, note that these are not ST products, and likely contain fake chips.
Can you reproduce this issue on a genuine ST board?
2026-03-20 6:08 AM
Part Number STM32F103CBT6TR (MCU IC)
Environment
Toolchain: STM32CubeIDE ( v1.18.0).
Debugger: ST‑Link
Hardware: Custom board based on STM32F103CBT6TR.
schematics: This is our own design, so we cannot share the full schematics publicly. However, the relevant connections are:
PA1 connected to LED (with series resistor).
Standard power supply and oscillator circuitry as per datasheet recommendations.
Internal RC oscillator used for initial testing
Details
Initially, when attempting to toggle GPIO pin PA1 using HAL functions (HAL_GPIO_TogglePin or HAL_GPIO_WritePin), the MCU immediately entered the HardFault handler after flashing.
Later, during debugging, instead of HardFault, the debugger reported a SIGTRAP (Trace/breakpoint trap).
Currently, stepping into HAL_Delay() leads to an IACCVIOL (Instruction Access Violation) fault.
Observed behavior: LED does not toggle, program halts in HardFault, SIGTRAP, or IACCVIOL depending on run/debug mode.
Debugger stack trace shows execution stuck in HAL_GetTick() inside HAL_Delay(), suggesting SysTick is not firing.
Expected Behavior: GPIO pin PA1 should toggle every 2000 ms using HAL_Delay, with no HardFault, SIGTRAP, or IACCVIOL errors.
Flash the following code on STM32F103CBT6TR custom board ,
Observe that after flashing, the MCU enters HardFault immediately, which result in toggle or led blink connected to it.
In debug mode, stepping into HAL_Delay triggers SIGTRAP with in fault analyzer, I see this one is getting on IACCVIOL, when like HAL_Delay line is getting executed in debug but before execution of delay, there is no fault seen in fault analyzer.
Sanity Checks
Verified GPIO initialization code matches CubeMX generated template.
Confirmed HAL_Init() and SystemClock_Config() are called before GPIO use.
Checked that SysTick interrupt is not firing (HAL tick not incrementing).
2026-03-20 6:10 AM
Can you reproduce this issue on a genuine ST board?
2026-03-20 6:22 AM
Well, I did the same this with the blue pill board. I used the STM32F103C8T6 while the one I am using in my project board is STM32F103CBT6TR which is pretty similar, I guess. So, I did flash the same toggle program for available pins in it, and I was able to see toggle on all pins which I configured.
2026-03-20 7:34 AM
As previously noted, a Blue Pill is most likely not a genuine STM32.
Have you tried this on a genuine ST board?
2026-03-20 5:43 PM
> HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_0);
> HAL_Delay(2000);
> Expected Behavior: GPIO pin PA1 should toggle every 2000 ms
Do you want to toggle PA0 or PA1?
This is effectively a repost from this:
Hard Fault Handler error in STM32F103CBT6TR - STMicroelectronics Community
The solution is the same: buy a board that works.
2026-03-20 11:16 PM - edited 2026-03-20 11:18 PM
Verify that BOOT0 pin is connected to ground - directly or via a resistor.
Also, if you are unsure about chip type (might be remarked F103C6) try to reduce RAM size in linker script to 10KiB.
2026-03-22 9:35 PM
I tried in NUCLEO-H753ZI development board too, but the toggle did happen for all selected board and its genuine like apart from the blue pill board STM32F103C8T6. Right now, I kind of suspect both the hardware design and the code too, so we are trying to analyze in both. Is there any other approach for this?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.