2019-04-23 5:52 AM
Hello,
should LSERDY assert with LSEBYP?
I have a SIT1533 (32.768 khz Mems ocsillator) connected to PC14/OSC32IN on a L412. I first reset the backup domain, than I enable LSEBYP and with next command I enable LSEON. On a cold start, where the SIT1533 may need 500 ms, LSERDY never asserts, also OSCIN is toggling when I check with a scope.
Otherwise why does the sequence
not set LSERDY?
2019-04-23 9:56 AM
Hello.
LSERDY indicates crystal's oscillation stability.
I didn't found any mentioned relationship between these two bits, but also is not mentioned the state of LSERDY in case of using external osc. (probably undefined)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.