2019-08-01 7:26 AM
I am using stm32F746. I have enabled the RTC via external oscillator using CubeMX.
The crystal is not connected. But I see that RTC is initialized without errors (no timeout) and LSERDY is 1. Manual says LSERDY is 1 when external oscillator is running.
How that could be possible?
2019-08-01 9:02 AM
Is the oscillator input pin of floating? It may pick up noise.
The LSERDY circuit is a counter, there's no discrimination for the frequency.
JW
2019-08-01 9:07 AM
That's kind of weird, a custom design? Things hung of PC13..15 ?
2019-08-01 9:09 AM
Thanks for reply. They are floating. I will try to ground them and check.
2019-08-01 11:36 AM
Better disable RCC_BCDR_LSEON and keep the LSE pins floating.
2019-08-11 9:48 AM
Hi all
I have checked that if both pins of oscillator are connected to the ground LSERDY is still set. A bit strange.
2019-08-11 11:17 PM
That indeed is.
Can you please output LSE to MCO1 and check if there are no oscillations?
You don't set LSEBYP, do you?
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.