2023-12-21 2:15 AM - edited 2023-12-21 2:20 AM
Good Morning Ladies and Gentlemen,
Could you communicate in a short way the size of the contact drill-holes (stm32f411 - CEU) ?
The diameter in AWG size would be enough.
We also are interested in further documentation-links regarding it.
In student words
"Have a nice day"
Solved! Go to Solution.
2023-12-21 6:41 AM
ST doesn't make that board, you'd need to ask the manufacturer.
But header pins plated through holes are typically around 1mm or 40mil, which is 18 AWG.
2023-12-21 2:21 AM
What is "contact drills"?
Are you talking about some of the development boards, e.g. Nucleo?
JW
2023-12-21 2:23 AM
"drillings"
2023-12-21 3:21 AM
"stm32f411ceu"
2023-12-21 3:39 AM
Hello @timbo2023 ,
Not sure I understood the question.
Could you please elaborate more or show image(s) or something similar to explain what you're talking about?
2023-12-21 3:43 AM
How many kind of holes to you see on a stm32f411ceu controller card?
Which diameter has this hole in "AWG-size"?
2023-12-21 5:15 AM
Do you mean this? https://stm32-base.org/boards/STM32F401CEU6-WeAct-Black-Pill-V3.0
JW
2023-12-21 5:19 AM
2023-12-21 6:41 AM
ST doesn't make that board, you'd need to ask the manufacturer.
But header pins plated through holes are typically around 1mm or 40mil, which is 18 AWG.
2023-12-21 6:42 AM
ok
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.