2022-06-13 5:57 AM
Hello good day!
I want to setup a CAN-FD message sending simulation with H7A3ZI-Q (one or two message ids). But i do not exactly know how to assemble the HW and what i need (For STM side). I know this board is capable of the CAN-FD but it needs a tranceiver. Is there already a board i can use for Pin PD0 and PD1 are the outputs of the CAN controller i want to connect.
For example I found this:
CAN FD 5 CLICK MIKROELEKTRONIKA - Click board | Transceiver; UART; UJA1162A; Prototypenplatine; MIKROE-4286 | TME - Elektronik Bauteile -> Where do I have to connect the RX/TX CAN output of the STM (5V+GND I would supply also)?
or a better alternative this:
CAN-Bus CAN FD Breakout Board. 5v Supply and 5v Logic (buyzero.de) -> here it is "just the TX and RX" to be connected.
Any advice from you experts?
Thanks!
2022-06-15 6:26 AM
Can be closed - solved.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.