2021-05-25 3:59 AM
Hello
I added a custom node and changed the default from the original code
(https://api.lb-0.testnet.chrysalis2.com/ ) ,but i noticed i get some error messages from the functions of the main menu .I would like to know if that has anything to do with the usertrust_thetangle.pem file , and if there is any specific configuration in the code for adding a custom node .
Thanks
2021-05-25 4:52 AM
Hello,
could you please provide the log messages you get on the serial terminal?
Thanks and regards
Andrea
2021-05-25 5:30 AM
When i try to send the sensor data to the tangle
{"Device":"B-L4S5I-IOT01A","time":1621853146,"temp":34.35,"humi":31.67}
Request:
GET /api/v1/tips HTTP/1.1
Host: iotabee.ddns.net
Content-Type: application/json
Request: POST /api/v1/messages HTTP/1.1
Host: iotabee.ddns.net
Content-Length: 533
Content-Type: application/json
Err response: access forbidden
message ID: 8z
2021-05-25 6:17 AM
Hello,
In my understanding, there is an issue with the message REST API on the Bee node side. In fact, if you try to use the "Client get info" test, it succeeds.
Regards
Andrea
2021-05-26 12:34 AM
Hello
Could you tell me what is the ACCOUNT_PATH which is defined in the test_config.h as #define ACCOUNT_PATH "m/44'/4218'/0'/0'" , and if that depends at any way with the TEST_NODE_ENDPOINT ?
Thanks
Dimitris
2021-05-26 1:13 AM
Hello
the ACCOUNT_PATH represents a base for the Address and Key generation as defined by BIP32 and BIP44 standards. This is included in the new IOTA 1.5 specification. The ACCOUNT_PATH is not related to the Node your Client interacts with.
Please, refer to the official Chrysalis documentation for further details on this topic.
Regards
Andrea
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.