2025-01-23 2:03 AM
Hi everyone,
I’m working on a custom board design using an STM32H753AII6 in the UFBGA169 package. I need to include external SDRAM but want to keep my PCB footprint as small as possible, so I’m leaning toward a BGA-packaged SDRAM rather than the typical TSOP.
Right now, I’m looking at the Micron MT48LC16M16A2B4-6A (which I believe is a 256 Mbit / 16-bit SDRAM, rated up to around 166 MHz). My plan is to run it in 16-bit mode at about 100–133 MHz using the STM32’s FMC SDRAM interface.
A few questions I have:
I’m fairly new to designing with BGA packages, so any advice or references to example schematics (especially using the STM32H7 in a BGA form factor) would be really appreciated. I have checked the STM32H753I-EVAL design, however it is using 32bit SDRAM rathern than a 16bit option.
Thank you in advance for your help!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.