2016-10-12 1:35 PM
We are using the following USB FS library. All I need is an additional IN end point to send data to Host. When I tried to add an End point, for end point 2, transfer complete flag is never set. When using End point 1 it is working fine. For End point 2: I can never clear the interrupt as transfer complete is never set. More over, I do not see any data sent to Host. Any help is really appreciated. if (diepint.b.emptyintr) { DCD_WriteEmptyTxFifo(pdev , epnum); CLEAR_IN_EP_INTR(epnum, emptyintr); } To add Endpoint: /** * @brief CustomHIDDevice_Init * Initialize the HID interface * @param pdev: device instance * @param cfgidx: Configuration index * @retval status */ static uint8_t CustomHIDDevice_Init (void *pdev, uint8_t cfgidx) { /* Open EP IN */ DCD_EP_Open((USB_OTG_CORE_HANDLE *)pdev, EP1_IN, 0x40, USB_OTG_EP_INT); /* Open EP IN */ DCD_EP_Open((USB_OTG_CORE_HANDLE *)pdev, EP2_IN, 0x40, USB_OTG_EP_INT); MyUSBDescriptor.Get_SerialNum(&MyConfigData.MyVars); return USBD_OK; } Any ideas or help really appreciated. Here is the library code version: ****************************************************************************** * @file usb_dcd_int.c * @author MCD Application Team * @version V2.1.0 * @date 19-March-2012 * @brief Peripheral Device interrupt subroutines #stm32f107
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.