2018-06-12 12:44 AM
Hello everyone,
I am looking for a board with a STM32F4 or any other microcontroller (STM32) with 2 CAN. The main issue I am facing, is finding a developpement board where the 2 CAN inputs/outputs are available (for example in the STM32F4 discovery board, one is connected to the USB, which doesn't suit me).
So if anyone knows a board that could fit my needs !
In advance, thanks !
#board #stm32f4 #can #development Note: this post was migrated and contained many threaded conversations, some content may be missing.2018-06-12 10:40 AM
What I meant is that I couldn't find the pins on the picture of the board (as I won't use the USB for example)
2018-06-12 10:43 AM
The Datasheet for the chips describe the pin options available, these may be further constrained by usage on the board in question.
>>However, this alternative still looks a bit expensive for me.
Really not providing constraining parameters here, the NUCELO/DISCO boards are artificially cheap, so if you start adding features, and need third-party boards, they are going to cost more. The boards here are relatively cheap compared to engineering time involved.
2018-06-12 10:58 AM
Provided that I only need 2 transceivers as additional boards, I still think this solution is cheaper than the RedDragon407
I am not saying that they are expensive regarding the engineering time involved, I am just looking for the cheapest way to developa link between two CAN buses.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.