2018-12-13 3:04 AM
I use AS4C8M32SA-6BIN on my board (https://www.alliancememory.com/wp-content/uploads/pdf/dram/Alliance%20Memory_256M%20SDRAM_AS4C8M32SA-6_7BIN(BCN)%20A%20die_rev%201.0%20November%202016.pdf)
But I get HardFault when I try to write to the address 0xD0000000
I don't understand what did wrong
Here's my code I removed all the unnecessary for clarity
// AS4C8M32SA-6BIN
#define SDRAM_MODEREG_BURST_LENGTH_1 ((uint16_t)0x0000)
#define SDRAM_MODEREG_BURST_LENGTH_2 ((uint16_t)0x0001)
#define SDRAM_MODEREG_BURST_LENGTH_4 ((uint16_t)0x0002)
#define SDRAM_MODEREG_BURST_LENGTH_8 ((uint16_t)0x0003)
#define SDRAM_MODEREG_BURST_TYPE_SEQUENTIAL ((uint16_t)0x0000)
#define SDRAM_MODEREG_BURST_TYPE_INTERLEAVED ((uint16_t)0x0008)
#define SDRAM_MODEREG_CAS_LATENCY_2 ((uint16_t)0x0020)
#define SDRAM_MODEREG_CAS_LATENCY_3 ((uint16_t)0x0030)
#define SDRAM_MODEREG_OPERATING_MODE_STANDARD ((uint16_t)0x0000)
#define SDRAM_MODEREG_WRITEBURST_MODE_PROGRAMMED ((uint16_t)0x0000)
#define SDRAM_MODEREG_WRITEBURST_MODE_SINGLE ((uint16_t)0x0200)
#define SDRAM_REFRESH_COUNT ((uint32_t)4096)
void SdramInitSequence() {
FMC_SDRAM_CommandTypeDef command;
command.CommandMode = FMC_SDRAM_CMD_CLK_ENABLE;
command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2;
command.AutoRefreshNumber = 1;
command.ModeRegisterDefinition = 0;
HAL_SDRAM_SendCommand(&hsdram1, &command, 0xFFFF);
HAL_Delay(1);
command.CommandMode = FMC_SDRAM_CMD_PALL;
command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2;
command.AutoRefreshNumber = 1;
command.ModeRegisterDefinition = 0;
HAL_SDRAM_SendCommand(&hsdram1, &command, 0xFFFF);
command.CommandMode = FMC_SDRAM_CMD_AUTOREFRESH_MODE;
command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2;
command.AutoRefreshNumber = 8;
command.ModeRegisterDefinition = 0;
HAL_SDRAM_SendCommand(&hsdram1, &command, 0xFFFF);
command.CommandMode = FMC_SDRAM_CMD_LOAD_MODE;
command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2;
command.AutoRefreshNumber = 1;
command.ModeRegisterDefinition =
SDRAM_MODEREG_BURST_LENGTH_1 | \
SDRAM_MODEREG_BURST_TYPE_SEQUENTIAL | \
SDRAM_MODEREG_CAS_LATENCY_2 | \
SDRAM_MODEREG_OPERATING_MODE_STANDARD | \
SDRAM_MODEREG_WRITEBURST_MODE_SINGLE;
HAL_SDRAM_SendCommand(&hsdram1, &command, 0xFFFF);
HAL_SDRAM_ProgramRefreshRate(&hsdram1, SDRAM_REFRESH_COUNT);
}
int main(void) {
MPU_Config();
SCB_EnableICache();
SCB_EnableDCache();
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_FMC_Init();
SdramInitSequence();
// HardFault
*(__IO uint32_t*)(0xD0000000) = 0xAFAFAFAF;
while(1);
}
static void MX_FMC_Init(void) {
FMC_SDRAM_TimingTypeDef SdramTiming;
/** Perform the SDRAM1 memory initialization sequence */
hsdram1.Instance = FMC_SDRAM_DEVICE;
/* hsdram1.Init */
hsdram1.Init.SDBank = FMC_SDRAM_BANK1;
hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_9;
hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_12;
hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_32;
hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;
hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_2;
hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE;
hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2;
hsdram1.Init.ReadBurst = MC_SDRAM_RBURST_ENABLE;
hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_0;
/* SdramTiming */
SdramTiming.LoadToActiveDelay = 2;
SdramTiming.ExitSelfRefreshDelay = 7;
SdramTiming.SelfRefreshTime = 7;
SdramTiming.RowCycleDelay = 6
SdramTiming.WriteRecoveryTime = 4;
SdramTiming.RPDelay = 3;
SdramTiming.RCDDelay = 3;
if (HAL_SDRAM_Init(&hsdram1, &SdramTiming) != HAL_OK) {
_Error_Handler(__FILE__, __LINE__);
}
}
void MPU_Config(void) {
MPU_Region_InitTypeDef MPU_InitStruct;
/* Disables the MPU */
HAL_MPU_Disable();
/**Initializes and configures the Region and the memory to be protected */
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.BaseAddress = 0xD0000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_32MB;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enables the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}
2021-08-25 6:44 AM
did you find the solution? I have a similar issue.
2021-08-25 8:12 AM
Isn't BANK1 at 0xC0000000 ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.