2014-09-29 9:34 PM
Hello Pro,
I want to save my data in to backup domain to backup data when reset happen ( watch dog timer reset). This is my code : uint16_t domua;// I wan to save this data. /* Configure the PVD Level to 2.9V */ PWR_PVDLevelConfig(PWR_PVDLevel_2V2); /* Enable PWR and BKP clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR | RCC_APB1Periph_BKP, ENABLE); /* Enable access backup and RTC */ PWR_BackupAccessCmd(ENABLE); domua=TIM_GetCounter(TIM2);// BKP_WriteBackupRegister(BKP_DR1, domua);// Back up data do mua. /***when watch dog timer reset, domua=0, At this time, I want to back up this data*/ if (domua==0){domua+=BKP_ReadBackupRegister(BKP_DR1);} But it doesn't work as I wish. Please help me point out what is going wrong ? Thanks a lot, Minh2014-10-01 2:55 AM
Have you connected a battery for the back up domain?
It will probably not work unless there is a battery connected. The documentation only implies this : ''Battery backup domain Backup domain description To retain the content of the RTC backup registers, backup SRAM, and supply the RTC when VDD is turned off, VBAT pin can be connected to an optional standby voltage supplied by a battery or by another source. To allow the RTC to operate even when the main digital supply (VDD) is turned off, the VBAT pin powers the following blocks: • The RTC • The LSE oscillator • The backup SRAM when the low-power backup regulator is enabled • PC13 to PC15 I/Os, plus PI8 I/O (when available) The switch to the VBAT supply is controlled by the power-down reset embedded in the Reset block.'' ''Backup domain reset The backup domain reset sets all RTC registers and the RCC_BDCR register to their reset values. The BKPSRAM is not affected by this reset. The only way of resetting the BKPSRAM is through the Flash interface by requesting a protection level change from 1 to 0. A backup domain reset is generated when one of the following events occurs: 1. Software reset, triggered by setting the BDRST bit in the RCC Backup domain control register (RCC_BDCR). 2. VDD or VBAT power on, if both supplies have previously been powered off.''We’re moving the ST Community to a new platform to give you a better and more reliable community experience.