2025-04-29 1:26 PM
Where can I find a copy of the source code?
Introduction to MB1971 LLC HAT 12 V to 7.5 V/1 A for F334 G474 Nucleo board - Application note
2025-04-29 1:38 PM
The document at the link you supplied says:
Before opening the STM32CubeMX ‘ioc’ file, make sure that the X-CUBE-DPOWER pack has been installed.
• Download the pack at https://www.st.com/en/embedded-software/x-cube-dpower.html
• Open the help tab and install the pack.
.
.
.
Once the pack has been installed, it is possible to check, change, modify the default workspace, and generate the
code for the IAR, Keil® or STM32CubeIDE compiler toolchains using the tab GENERATE CODE in the main
interface.
2025-04-30 6:52 PM
I have installed the DPower pack, but where can I find the sample project file?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.