2016-09-10 10:17 AM
The main question is how to run two motors
SecondMotorRotateToLeft() and FirstMotorRotateToLeft()
in the same time?#include ''stm32f10x.h''
#include ''stm32f10x_gpio.h''
#include ''stm32f10x_rcc.h''
void Delay(unsigned int t)
{
unsigned int i;
for (i=0;i<t;i++);
}
void GPIOD_Initialize(){
GPIO_InitTypeDef GPIOC_Stepper;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC|RCC_APB2Periph_GPIOD, ENABLE);
GPIOC_Stepper.GPIO_Pin=GPIO_Pin_1|GPIO_Pin_3|GPIO_Pin_5|GPIO_Pin_7;
GPIOC_Stepper.GPIO_Mode=GPIO_Mode_Out_PP;
GPIOC_Stepper.GPIO_Speed= GPIO_Speed_50MHz;
GPIO_Init(GPIOC,&GPIOC_Stepper);
GPIO_InitTypeDef GPIOD_Stepper;
GPIOD_Stepper.GPIO_Pin=GPIO_Pin_1|GPIO_Pin_3|GPIO_Pin_5|GPIO_Pin_7;
GPIOD_Stepper.GPIO_Mode=GPIO_Mode_Out_PP;
GPIOD_Stepper.GPIO_Speed= GPIO_Speed_50MHz;
GPIO_Init(GPIOD,&GPIOD_Stepper);
}
void SecondMotorRotateToLeft()
{
GPIO_Write(GPIOD,GPIO_Pin_5);
Delay(time);
GPIO_Write(GPIOD,GPIO_Pin_5| GPIO_Pin_3);
Delay(time);
GPIO_Write(GPIOD,GPIO_Pin_3);
Delay(time);
GPIO_Write(GPIOD,GPIO_Pin_3|GPIO_Pin_7);
Delay(time);
GPIO_Write(GPIOD,GPIO_Pin_7);
Delay(time);
GPIO_Write(GPIOD,GPIO_Pin_7|GPIO_Pin_1);
Delay(time);
GPIO_Write(GPIOD,GPIO_Pin_1);
Delay(time);
GPIO_Write(GPIOD,GPIO_Pin_1|GPIO_Pin_5);
Delay(time);
}
void FirstMotorRotateToLeft()
{
GPIO_Write(GPIOC,GPIO_Pin_5);
Delay(time);
GPIO_Write(GPIOC,GPIO_Pin_5| GPIO_Pin_3);
Delay(time);
GPIO_Write(GPIOC,GPIO_Pin_3);
Delay(time);
GPIO_Write(GPIOC,GPIO_Pin_3|GPIO_Pin_7);
Delay(time);
GPIO_Write(GPIOC,GPIO_Pin_7);
Delay(time);
GPIO_Write(GPIOC,GPIO_Pin_7|GPIO_Pin_1);
Delay(time);
GPIO_Write(GPIOC,GPIO_Pin_1);
Delay(time);
GPIO_Write(GPIOC,GPIO_Pin_1|GPIO_Pin_5);
Delay(time);
}
int main(void)
{
const int time = 10000;
GPIOD_Initialize();
while(1)
{
FirstMotorRotateToLeft();
SecondMotorRotateToLeft();
}
}
2016-09-10 1:53 PM
Well, you need to get rid of Delay() and learn how to use timer interrupts, but a rudimentary version for quick testing might be perhaps like this:
void BothMotorsRotateToLeft()
{ GPIO_Write(GPIOC,GPIO_Pin_5); GPIO_Write(GPIOD,GPIO_Pin_5);Delay(time);
GPIO_Write(GPIOC,GPIO_Pin_5| GPIO_Pin_3); GPIO_Write(GPIOD,GPIO_Pin_5| GPIO_Pin_3); Delay(time); GPIO_Write(GPIOC,GPIO_Pin_3); GPIO_Write(GPIOD,GPIO_Pin_3); Delay(time); GPIO_Write(GPIOC,GPIO_Pin_3|GPIO_Pin_7); GPIO_Write(GPIOD,GPIO_Pin_3|GPIO_Pin_7);Delay(time);
GPIO_Write(GPIOC,GPIO_Pin_7); GPIO_Write(GPIOD,GPIO_Pin_7);Delay(time);
GPIO_Write(GPIOC,GPIO_Pin_7|GPIO_Pin_1); GPIO_Write(GPIOD,GPIO_Pin_7|GPIO_Pin_1);Delay(time);
GPIO_Write(GPIOC,GPIO_Pin_1); GPIO_Write(GPIOD,GPIO_Pin_1); Delay(time); GPIO_Write(GPIOC,GPIO_Pin_1|GPIO_Pin_5); GPIO_Write(GPIOD,GPIO_Pin_1|GPIO_Pin_5);Delay(time);
} JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.