2024-09-02 8:51 PM
As shown in the screenshot below. RUN_PD bit is mentioned here and nowhere else in the entire Reference manual.
2024-09-02 10:13 PM - edited 2024-09-05 4:48 AM
Hello @KSB
Thank you so much for reporting this issue. I've escalated to the concerned team for correction on the coming release of the document (under internal ticket number 190285).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-01 12:21 PM
Hello @STTwo-32,
When will RM0503 be updated to clarify support for a RUN_PD bit? Can you at least confirm if this functionality is supported? I am prototyping a project now that may depend on this feature.
Regards,
Clyne
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.