2016-10-13 8:02 AM
Hi,
I�m using the STM32F4 Discovery TIMER3 with channel 1 and channel 3 in mode pwm output. I realised that when I�m use the module timer, I get ringing noise in the rising edge and falling edge of the PWM, and also in the VDD. Also I watched in an osciloscope that this noise adds in the others channels of the timer too. Is there a solution to eliminate that noise? I used my code and the example code for the discovery (official). Thanks for advance. Leonardo #stm32f4-pwm-output-noise2016-10-13 8:22 AM
If you are generating 50Hz PWM signals don't set the pin driver slew rate to 25-100 MHz? Pick something that is appropriate to the speed and loading you have.
2016-10-13 8:36 PM
What clive said.
Also, you could try adding a small series resistor and cap to ground to damp the ringing a little. Something in the range 47-220R and 10-100pF might do it.2016-10-14 12:37 PM
First at all, thanks Clive1.
I forgot to mention that the frequency of the PWM is 500 KHz and the pin driver with slew rate to 25 to 100 MHz in Pull-up mode.The PWM output controls a H bridge (DRV592A) with an LC output
filter.
I think the probe of the oscilloscope is adding the noise.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.