2015-07-29 7:59 AM
Hi,
I have an STM32L15x. Is it possible to reset the microcontroller only over SWCLK and SWDIO without the reset pin when the microcontroller is in standby mode? I can access the target ID over SWD even though the device is in standby so I suppose the debug unit is not completely powered down. Programming or debugging however is not possible. The use case is a product that is programmable over SWD but with as few connectors to outside as possible. #stm32-swd-reset-standbyWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.