2023-09-13 5:25 AM
Hi,
I'm using USART with DMA to transmit a fixed sized packet message from master to slave, and have the slave send back a fixed size response. I have a freeRTOS enabled. I have DMA setup in circular mode, and set the buffer size to twice the size of the largest packet size I expect to receive, in case of an overflow which is unlikely to happen. This all works well but would like to improve my solution to avoid having a freeRTOS task on the slave block for a short time when it sends a response.
How do I reset the USART DMA's rx buffer memory pointer to DMA_CMAR's initial programmed value?
I currently send a response and reset the USART/DMA on the slave after it receives a request from the master like this:
HAL_UART_Transmit(&huart2, (uint8_t*)txData, 4, HAL_MAX_DELAY);
HAL_UART_DMAStop(&huart2);
HAL_UART_Receive_DMA(&huart2, clock_USART_DMA_RX_Buffer, CLOCK_PACKET_MAX_LENGTH * 2);
I would like to do something like the following instead, but when I transmit from the
slave using DMA, I need to block the freeRTOS task to wait until the slave UART is
done transmitting back to the master. If I don't wait, the transmission gets cut off early
when DMA is stopped:
HAL_UART_Transmit_DMA(&huart2, (uint8_t*)txData, 4);
// need to poll DMA Transfer Complete here.... which blocks freeRTOS task
HAL_UART_DMAStop(&huart2);
HAL_UART_Receive_DMA(&huart2, clock_USART_DMA_RX_Buffer, CLOCK_PACKET_MAX_LENGTH * 2);
Thank you
2023-09-13 6:27 PM
Why are you calling HAL_UART_DMAStop at all? The transmission will stop when it's complete, no need to wait around until it does. You could also call it prior to HAL_UART_Transmit_DMA and start the RX and TX at the same time, if you really wanted.
In terms of receiving, setting up a circular buffer and processing data as it comes in is the most robust solution, rather than stopping/starting RX all the time. You can use the idle/HT/TC interrupts to process data appropriately.
2023-09-13
11:39 PM
- last edited on
2023-09-14
1:10 AM
by
Lina_DABASINSKA
So now you have to learn asynchronous and multi-thread software design and development. In other words, you "just" have to learn the actual software engineering, because your current level of understanding is on a level of Arduino and HAL/Cube team.
As for the reception: https://github.com/MaJerle/stm32-usart-uart-dma-rx-tx
@Guenael Cadier will gladly tell you how "easy" all of it is with the "competently designed and useful" HAL library!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.