2011-07-22 12:04 AM
Hi,
I have the following problem. I have a RFID-Reader Chips from Melexis (90109) connected to two GPIO Pins (Clock and Data). I process the incoming data with an EXTI handler that is triggert on the falling edge of the clock pin. This works fine. To detect if a transponder has left the field I must detect if the clock line is no longer atcive for a certain amount of time. My current approach is that I set up TIM2 as normal Timebase counter with an TIM_UPDATE IRQ-Handler as sort of watch dog for the clock line. In the EXTI handler I tried to reset TIM2 with TIM_SetCounter(TIM2, 0); so that as long as I receive clock pulses shorter than the timer period, the TIM2 Handler should not be called at all. If the clock stops, TIM2 handler should set a flag to signals the main loop that the transponder was removed. So far the idea, but reality shows that although I reset the TIM2 counter regulary I always get the TIM2 IRQ in it's normal period. Do I have to reset/restart a timer in a different way? Best Tom2011-07-23 11:29 AM
Please post your TIM2 configuration
2011-07-25 2:03 AM
Hi,
here is my TIM2 config// Timer to detect if transponder was removed
#define
TIMER_TAKT10000
/* Timer wird mit 10kHz getaktet */
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; uint16_t PrescalerValue; RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);// TIMER 2 Takt freigeben
PrescalerValue = (uint16_t) (SystemCoreClock / TIMER_TAKT) -1
;// Vorteiler berechnen
// Timer Grundkonfiguration
TIM_TimeBaseStructure.TIM_Period =100
;// Timer zählt von 0 ... 100: also alle 10ms
TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue; TIM_TimeBaseStructure.TIM_ClockDivision =0
; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);// Timer einstellen
//Timer Vorteiler-Taktkonfiguration
TIM_PrescalerConfig(TIM2, PrescalerValue, TIM_PSCReloadMode_Immediate);// Auto-Reload
// Timer aktivieren
TIM_Cmd(TIM2, ENABLE); NVIC_InitTypeDef NVIC_InitStructure;/* Enable the Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority =0
; NVIC_InitStructure.NVIC_IRQChannelSubPriority =1
; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE); I attach an Screenshot of my LA, where you can see the clock in wich EXTI doTIM_SetCounter(TIM2,
0
);// reset watchdog counter as we still receive clock ticks
In the timer IRQ handler I toggle an IO port, which you can see in the bottom line: Best Tom ________________ Attachments : Timer-Reset.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0rh&d=%2Fa%2F0X0000000bh5%2FPh6rP86fHT35bOaqG049yYz0VZ45GVztBJnFD5uCOfc&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.