2011-07-24 3:52 AM
Hi,
My application would only run when I provide an external reset to my board (but when I use a JTAG debugger, it seems to work fine).
Is this a problem with the embedded power on reset? Do I need a delay at power-up?
2011-07-24 11:16 PM
Please check the h/w connections like VDD and GND tracks on the board.
2011-07-25 12:07 AM
Hi,
The problem was with the boot pins. There was a capacitor connected to one of the boot pins. This caused an incorrect value to be latched on the 4th rising edge of the system clock after reset.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.