2011-07-24 3:40 PM
Hi All,
I am trying to change RTC->PRLH and RTC->PRLL.
The second WHILE hangs.
I keep re-reading the same paragraph in the STM32F101xx reference manual (UM0306, CH8), but I can't see what I am doing wrong.
Preceding code has enabled APB1 at much more than 4x 32kHz.
Commenting out the second WHILE and reading RTC->PRLL later confirms that it has been set as expected.
Thoughts please.
-Mark
while((RTC->CRL & RTC_CRL_RTOFF) ==0);
RTC->CRL |=RTC_CRL_CNF;
RTC->PRLH =0;
RTC->PRLL =0x7FFF;
RTC->CRL &=~RTC_CRL_CNF;
while((RTC->CRL & RTC_CRL_RTOFF) == 0);
2011-07-24 10:43 PM
You need to enable the RTC clock first.
Here's a sample code:
// enables the clock to Backup and power interface peripherals
RCC_APB1PeriphClockCmd(RCC_APB1Periph_BKP | RCC_APB1Periph_PWR,ENABLE);
// enables acces to BKP and RTC registers
PWR_BackupAccessCmd(ENABLE);
// enable 32.768 kHz external oscillator
RCC_LSEConfig(RCC_LSE_ON);
// provide delay to stabilize LSE
delay(5000);
// set LSE as RTC clock source
RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE);
// enable RTC clock
RCC_RTCCLKCmd(ENABLE);
//RTC_WaitForLastTask();
// wait for register sync
//RTC_WaitForSynchro();
RTC_WaitForLastTask();
// set RTC prescaler
RTC_SetPrescaler(USED_RTC_XTAL_FREQ-1);
RTC_WaitForLastTask();
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.