2016-06-22 9:45 AM
Hello
I have a STM32F429I - DISC1 microcontrollers. After mishandling likely, the microcontroller was not started.
When I plug in the USB cable, my computer tells me that the device is not working properly. The only LEDs that are turned on are:
- G2 ((red) for 3.3 V power-on)
- LD6 ((RED) OC (over- current))
Is it possible to reset the microcontroller or reboot?
Thank you
2016-06-22 9:59 AM
Physical damage is not something you can fix with a button.
If you have loaded some broken software you can strap BOOT(0) to VDD and have the device boot into the system Loader, from where you can erase the errant code.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.