STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0xx ADC MAX Vref and Converted Value

Posted on June 22, 2016 at 18:29It is recommended to use DMA for multiple ADC channels, and I spent too much time trying to switch between channels manually. So I used STM32CubeMX to get DMA working for ADC1_Channel_0 and Channe_1 It seems with 3V3 ...

gerhard by Associate II
  • 675 Views
  • 1 replies
  • 0 kudos

STM32F0xx ADC oversampling with DMA

Posted on June 22, 2016 at 18:47It is recommended to use DMA for multiple ADC channels, and I spent too much time trying to switch between channels manually. So I used STM32CubeMX to get DMA working for ADC1_Channel_0 and Channe_1 I want to take x16...

gerhard by Associate II
  • 845 Views
  • 0 replies
  • 0 kudos

SPI link max speed between two STM32 of different families

Posted on June 22, 2016 at 16:32Hi all, I have two boards which are respectively including an STM32F429 and an STM32F303. I want to achieve a SPI link between those boards with these following features. - STM32F429 is master; STM32F303 is slave - ST...

sylvain2 by Associate
  • 1363 Views
  • 1 replies
  • 0 kudos

STM Timer OC Polarity runtime change

Posted on January 14, 2016 at 15:38 Hi, I have setup a OnePulse mode on a channel of a STM32F446 Timer TIM5_CH1 : void TIM_MS_Init(void) { TIM_OC_InitTypeDef sConfigOC; /* Compute the prescaler value to have TIM5 counter clock equa...

DAC triangle waveform: DHR polluted, wrong output amplitude

Posted on June 22, 2016 at 15:31Hi again,In my never-ending quest to understand the registers, I try some changes in the code I had to output a triangle waveform from DAC channel2 on STM32 F334R8.I have several questions.- I use PA_05 to output my s...

0690X00000605N6QAI.png
antoine by Associate II
  • 630 Views
  • 0 replies
  • 0 kudos

[STM32L4] Bit banding

Posted on June 15, 2016 at 10:27Hi,I want to use the Bit Banding region of STM32L4 but I do not know how to modify the linker script for the same.I tried to follow the https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?Roo...

sunny by Associate II
  • 3958 Views
  • 11 replies
  • 0 kudos

STM32f429I crashes when activating TIM8

Posted on April 20, 2016 at 17:53Hi, I am using a STM32F429I discovery board and I would like to use the TIM8 with external clock source to trigger ADC conversions. Unfortunately, when I activate and configure TIM8 in STM32CubeMX my application cras...

smrtkai by Senior
  • 3129 Views
  • 11 replies
  • 0 kudos

STM32F767ZI Nucle-144: Higher frequency than 180Mhz.

Posted on June 19, 2016 at 17:16Hi everyone, I am configuring my system_stm32f7xx.c file and I noticed while looking through the reference manual that the max PLL frequency is only 180Mhz. I am looking to get 192Mhz. Does anyone know how to get more...

Configuring SDADC for Repeat Triggering with DMA

Posted on June 22, 2016 at 06:36I need SDADC1 to do a scanned injected DMA conversion of fifty samples total each time there is a TRGO output from TIM4. I have confirmed by measurement using HAL_GetTick() that TIM4 is cycling at the desired rate of ...

spflanze by Associate II
  • 1044 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.