2008-10-05 8:15 PM
remap PD 0 and 1 - to GPIO inputs
2011-05-17 3:46 AM
2011-05-17 3:46 AM
Hi,
I see there were some problems with the remap feature for PD0/PD1, but STone says it is fixed in the release silicon. I am trying to use PD0 and PD1 as GPIO, input, pull-up. It does not seam to work - they are always read as zero, even with nothing connected (and it is configured with the pull-up). Has anyone done this successfully, and can they let me see the code they used to do it ? Thanks. I currently have :- GPIO_PinRemapConfig(GPIO_Remap_PD01, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOD, ENABLE); GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU; GPIO_Init(GPIOD, &GPIO_InitStructure); Thanks, John. [ This message was edited by: john.walsh on 01-10-2008 11:21 ]2011-05-17 3:46 AM
2011-05-17 3:46 AM
which package of microcontroller do u use?
is this eval board? This is available only on 36-, 48- and 64-pin packages (PD0 and PD1 are available on 100-pin and 144-pin packages, no need for remapping). if it is ok then check the bit 15 in the register AFIO_MAPR.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.