2017-10-04 9:15 AM
Reading the reference manual of STM32F4xx (RM0090), I need some explanation about the physical remap in FMC.
Page 71-72, �2.4, the interpretation of table 4 is not clear. Should I understand that when in mode Remap in FMC:
if MEM_MODE=010b (SYSCFG �9.3.1 page 298) :
NOR/PSRAM bank1 (64MB) goes from 0x0000 0000 to 0x03FF FFFF
and
NOR/PSRAM bank2 (64MB) goes from 0x0400 0000 to 0x07FF FFFF
and if MEM_MODE=100b (SYSCFG �9.3.1 page 298) :
the lower 128MB (out of 256MB) of SDRAM 1 are mapped from 0x0000 0000 to 0x07FF FFFF
(and the upper 128MB of SDRAM 1 are not accessible)
Because what I read in Table 4 doesn't look logical / correct. How does it exactly work ?
Thank you !
#stm32f4 #fmc #remap2017-10-05 1:32 AM
Hello Christophe,
can you please provide more info what does not look correct to you?
Best regards,
Tilen
2017-10-05 4:52 AM
Hello Tilen,
Table 4, page 72, when Remap in FMC mode:
* memory section 1, range 0x0400 0000 - 0x07FF FFFF: FMC bank 1 NOR/PSRAM 2 (128 MB aliased)
This range is 64MB.
NOR/PSRAM 2 is 64MB too and then can be remapped there. So Why this comment about '128 MB aliased' ?
* memory section 0, range 0x0000 0000 - 0x03FF FFFF: FMC bank 1 NOR/PSRAM 1 (128 MB aliased)
or FMC SDRAM bank 1 (128 MB aliased)
This range is also 64MB.
It can be mapped to PSRAM 1 which is also 64 MB. So why is it noted '128MB aliased' ?
With FMC SDRAM bank 1 (which is 256 MB), if 128MB are aliased, it should map both blocs (0x0000 0000 - 0x07FF FFFF).
Then only half of the 256MB SDRAM bank 1 can be mapped (I assume that this is the lower part). So why there is no reference to SDRAM bank 1 in the comment of memory section 1 (0x0400 0000 - 0x07FF FFFF) ?
Regards,
Christophe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.