2017-06-03 5:07 AM
hi,
Is CPU halt when DMA access the bus for data transfer between peripheral and memory? if it is true then why in Application note AN4031 they have written
''The DMA allows data transfers to take place in the background, without the intervention of
the Cortex-Mx processor. During this operation, the main processor can execute other tasksand it is only interrupted when a whole data block is available for processing.'because if CPU halts, then it doesn't matter whether CPU resources are free or not...
thanks
#stm32f4 #dma #an4031We’re moving the ST Community to a new platform to give you a better and more reliable community experience.