2013-01-24 4:05 PM
I have designed a custom board around STM32F407VET. I am using 8 MHz external oscillator (ABRACON ABLS-8.000MHZ-B2-T) with 22 pf load capacitors (CL) and 220 ohm REXT. When I probe OSC_IN or OSC_OUT pins using logic analyzer I see no oscillation. I have tried various values of CL from 18 pf to 27 pf and REXT from 120 to 470 ohm with no success. I measure the correct frequeny on STMF4 Discovery kit with my set up. Since external oscillator is not working the microcontroller automatically switches to internal oscillator and I am able to program the board. However, I would like to use the external oscillator as planned. I would appreciate if someone can recommend oscillator part number, CL and REXT values that they have used in the past and are known to work with STM32F4xx series.
Thanks.2013-01-24 6:33 PM
The part starts with the HSI, it has to have the HSE enabled manually, do you have software on it doing that? The Discovery board has a 20pF crystal. The Abracon is 22pF, 80 Ohm ESR, most recommended by ST seem to be 20pF or less.
You could also try a 0 Ohm. The lead length also needs to be very short. Perhaps you can provide a gerber fragment of the topology. Consider also the impact of scope probes to the circuit.2013-01-24 10:36 PM
''I probe OSC_IN or OSC_OUT pins using logic analyzer''
You should be using an Oscilloscope to look at those - they are analogue signals!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.