2022-04-13 5:26 AM
I took the stm32Cube example : Projects\STM32L562E-DK\Examples\OCTOSPI\OSPI_NOR_ReadWrite_DMA and modified it to send a RDID (9Fh) instruction to the NOR. I get a "0xAC 0x28 0x53" but I ignore which codes that NOR flash is supposed to answer. It could be valid, though.
Then, I send a RDSDFP instruction (5Ah) and then I receive a sequence of "0x00" which is wrong because the NOR flash is supposed to send 0x50444653.
Could someone share the code functions using a simple OSPI_RegularCmdTypeDef to read the NOR-flash ID and the NOR-flash SDFP So that I can verify on my disco kit that the NOR-flash is alive.
Thanks
Solved! Go to Solution.
2022-04-13 6:50 AM
Ok for that RDID , restoring the bitorder give a coherent " C2 85 3A "
I still cannot get the a correct SDFP (but now always a sequence of 0xFF)
2022-04-13 5:35 AM
for info:
static void OSPI_Read_NOR_ID(OSPI_HandleTypeDef *hospi)
{
OSPI_RegularCmdTypeDef sCommand;
sCommand.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
sCommand.FlashId = HAL_OSPI_FLASH_ID_1;
sCommand.Instruction = 0x9F;
sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS;
sCommand.AddressMode = HAL_OSPI_ADDRESS_NONE;
sCommand.DataMode = HAL_OSPI_DATA_1_LINE;
sCommand.DummyCycles = 8;
sCommand.DQSMode = HAL_OSPI_DQS_DISABLE;
sCommand.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
sCommand.NbData = 3;
if (HAL_OSPI_Command(hospi, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_OSPI_Receive(hospi, aRxBuffer, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
}
static void OSPI_Read_SFDP(OSPI_HandleTypeDef *hospi)
{
OSPI_RegularCmdTypeDef sCommand;
sCommand.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
sCommand.FlashId = HAL_OSPI_FLASH_ID_1;
sCommand.Instruction = 0x5A;
sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS;
sCommand.DataMode = HAL_OSPI_DATA_1_LINE;
sCommand.DummyCycles = 8;
sCommand.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
sCommand.AddressMode = HAL_OSPI_ADDRESS_1_LINE;
sCommand.AddressSize = HAL_OSPI_ADDRESS_24_BITS;
sCommand.Address = 0;
sCommand.NbData = 0x18;
if (HAL_OSPI_Command(hospi, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
if (HAL_OSPI_Receive(hospi, aRxBuffer, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
}What could be wrong ?
2022-04-13 5:38 AM
2022-04-13 5:52 AM
>> I get a "0xAC 0x28 0x53" but I ignore which codes that NOR flash is supposed to answer
For the ReadID the digits you're getting are shifted... Check table 15 in the documentation.
2022-04-13 6:50 AM
Ok for that RDID , restoring the bitorder give a coherent " C2 85 3A "
I still cannot get the a correct SDFP (but now always a sequence of 0xFF)
2022-04-14 8:01 AM
Sending The SFDP command (0x5A) in a regular command:
sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS;
sCommand.DataMode = HAL_OSPI_DATA_1_LINE;
sCommand.DummyCycles = 8;
sCommand.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
sCommand.AddressMode = HAL_OSPI_ADDRESS_1_LINE;
sCommand.AddressSize = HAL_OSPI_ADDRESS_24_BITS;and the 0x50444653 is expected from the NOR flash.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.