2026-04-29 6:34 AM
I am using an stm32u585, specifically the b-u585i-iot02a development kit board.
I set up a basic project using stm32cube ide to test clock configurations. System is clocked from the MSIS at 24MHz with PSC of 1 -> HCLK is 24MHz.
I enabled the RNG peripheral, clocked with the HSI48. In the default SystemClock_Config() function I commented out the code related to enabling the HSI48. RNG initialization is left as default.
Interestingly, the RNG can still generate random numbers with HAL_RNG_GenerateRandomNumber(). The MX_RNG_Init() function succeeds as well.
Reading HSI48ON and HSI48RDY bits from the status registers give both values as 0.
How is the RNG still working and generating valid numbers?
Another curiosity: In this state, the whole MCU takes less power than if I leave the SystemClock_Config() as generated (explicitly enabling the HSI48).
See code snippets below:
System clock config
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE3) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
// RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_MSI;
// RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_1;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_PCLK3;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}RNG init
/**
* @brief RNG Initialization Function
* @PAram None
* @retval None
*/
static void MX_RNG_Init(void)
{
/* USER CODE BEGIN RNG_Init 0 */
/* USER CODE END RNG_Init 0 */
/* USER CODE BEGIN RNG_Init 1 */
/* USER CODE END RNG_Init 1 */
hrng.Instance = RNG;
hrng.Init.ClockErrorDetection = RNG_CED_ENABLE;
if (HAL_RNG_Init(&hrng) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN RNG_Init 2 */
/* USER CODE END RNG_Init 2 */
}
Checking status
volatile uint32_t rng_src=__HAL_RCC_GET_RNG_SOURCE(); // 0 => HSI48
volatile uint32_t hsi48_on = (READ_BIT(RCC->CR, RCC_CR_HSI48ON) != 0U);
volatile uint32_t hsi48_rdy= __HAL_RCC_GET_FLAG(RCC_FLAG_HSI48RDY);
volatile uint32_t drdy = __HAL_RNG_GET_FLAG(&hrng, RNG_FLAG_DRDY);
volatile uint32_t sr = RNG->SR; // check CECS/SECS bits
random32 = 0;
HAL_StatusTypeDef st = HAL_RNG_GenerateRandomNumber(&hrng, &random32);
volatile uint32_t err = HAL_RNG_GetError(&hrng);
if(st != HAL_OK)
{
__NOP();
}
clock configuration:
2026-05-03 2:55 AM
you can check the RNGSEL field in the RCC peripheral clock selection register, whether it is select the HSI48
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.