2025-01-14 2:22 AM
Hello and thanks in advance for reading my post.
I am currently working on my dissertation, trying to implement a digital signing algorithm on a Arm Cortex-M0+ microprocessor. I'm using a NUCLEO-G0B1RE board with a stm32 with the same series. This board does not come with a TRNG peripheral and I don't want to use a packaged one, as I'm trying to understand the process of crceating an RNG as well.
From some posts I have read (either on this forum or other ones), it seems that uninitialized SRAM is a good starting point for my entropy source. I'm also taking into consideration using time jitter between two oscillators (mainly the 32 kHz +- 5% RC oscillator and the PLL block).
I use VSCode and I wrote my own linker script and startup code.
I have created a noinit section that loads into SRAM:
.noinit (NOLOAD) : {
*(.noinit)
} >SRAMSRAM is a memory zone which has the origin and length based on the memory organization chapter in the reference manual and is according to my device specifications:
SRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 144KI have also created a volatile array of unsigned integers to be loaded in the noinit section:
volatile uint8_t au8Arr[1024] __attribute__((section(".noinit")));When using Cortex-Debugger to check the values inside au8Arr in the Reset_Handler, there seems to be very little if any modification at all in bytes.
It seems that SRAM is retained even on longer power cycles (1min - 10min).
My question is how can I make the retention period much smaller (if none at all) or how can I adapt to these behaviour?
Solved! Go to Solution.
2025-01-14 3:05 AM - edited 2025-04-16 8:32 AM
As it says in your 1st link, the randomness is "biased" by process variations - I don't think it's safe to assume that "bias" won't completely swamp other random effects?
@undacmic wrote:
- Temperature sensor LSB? (it just seems that it is susceptible to external alterations of temperature that might result in pretty stable ADC reads)
That's why you consider only the LSB - that's always going to be the least stable.
@undacmic wrote:
- Time jitter?
Yes, that's a common one
@undacmic wrote:
- What can I do to read the analogue values within the memory array?
Nothing - that's hidden by the hardware.
@undacmic wrote:
- Any other way?
Yes, many - what's practical/useful depends on the specific application.
If there were just one, simple, universal way - then chipmakers wouldn't have to go to lengths to provide TRNGs!
2025-01-14 2:39 AM - edited 2025-01-14 2:40 AM
@undacmic wrote:From some posts I have read (either on this forum or other ones), it seems that uninitialized SRAM is a good starting point for my entropy source
I don't think so - perhaps you are misinterpreting those posts?
While there are some proposals that do use uninitialised memory, I think they look at the analogue values within the memory array?
What you read via software is quantised into just '1' or 'zero' - so you lose the vast majority of the entropy.
The digital values that code reads from uninitialised memory do tend to be pretty constant.
2025-01-14 2:53 AM
Honestly, it is my first time doing an embedded project and I might be misguided, but here is a list of what I've found, again I am not saying this is a correct implementation, is just that some other people seem to have tried, and using NIST statistical tests to prove the usability of the entropy source seemed good for me:
Ok, now let's say this is an incorrect assumption, what approach I should take for using only the board for entropy?
2025-01-14 3:05 AM - edited 2025-04-16 8:32 AM
As it says in your 1st link, the randomness is "biased" by process variations - I don't think it's safe to assume that "bias" won't completely swamp other random effects?
@undacmic wrote:
- Temperature sensor LSB? (it just seems that it is susceptible to external alterations of temperature that might result in pretty stable ADC reads)
That's why you consider only the LSB - that's always going to be the least stable.
@undacmic wrote:
- Time jitter?
Yes, that's a common one
@undacmic wrote:
- What can I do to read the analogue values within the memory array?
Nothing - that's hidden by the hardware.
@undacmic wrote:
- Any other way?
Yes, many - what's practical/useful depends on the specific application.
If there were just one, simple, universal way - then chipmakers wouldn't have to go to lengths to provide TRNGs!
2025-01-14 3:14 AM
Yes, many - what's practical/useful depends on the specific application.
If there were just one, simple, universal way - then chipmakers would have to go to lengths to provide TRNGs!
I think it's out of topic to mention, but just for context, I'm looking into a SPHINCS+ implementation, which needs some secret keys created using a PRF. I was thinking to use a hash algorithm for this, but I wanted to hash an "as random as possible" value.
@undacmic wrote:
- Time jitter?
Yes, that's a common one
Ok, I will try two approaches and benchmark my results.
One using multiple floating ADC pins on which I will try to apply some bit-wise operation.
The other using time jitter, but regarding this I have one more question.
To obtain good results (which I think should mean as much jitter as possible) which on-board clock blocks/oscillators I should use, and bigger frequency is equal to higher jitter?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.