2019-12-23 9:10 AM
Using HAL. How to read unique ID and use it to identify specyfic chip?
Do simple:
uint32_t HAL_GetREVID (void )
uint32_t HAL_GetDEVID (void )
Do the job? Are they really unique, or can these values repeat in same chips?
Solved! Go to Solution.
2019-12-23 9:39 AM
No, those relate to the type/step of IC you have ie H743 Step V
The Unique is pulled as 3x 32-bit values from memory
#define UID_BASE (0x1FFF7590UL) /*!< Unique device ID register base address */
/**
* @brief Get Word0 of the unique device identifier (UID based on 96 bits)
* @retval UID[31:0]: X and Y coordinates on the wafer expressed in BCD format
*/
__STATIC_INLINE uint32_t LL_GetUID_Word0(void)
{
return (uint32_t)(READ_REG(*((uint32_t *)UID_BASE_ADDRESS)));
}
/**
* @brief Get Word1 of the unique device identifier (UID based on 96 bits)
* @retval UID[63:32]: Wafer number (UID[39:32]) & LOT_NUM[23:0] (UID[63:40])
*/
__STATIC_INLINE uint32_t LL_GetUID_Word1(void)
{
return (uint32_t)(READ_REG(*((uint32_t *)(UID_BASE_ADDRESS + 4U))));
}
/**
* @brief Get Word2 of the unique device identifier (UID based on 96 bits)
* @retval UID[95:64]: Lot number (ASCII encoded) - LOT_NUM[55:24]
*/
__STATIC_INLINE uint32_t LL_GetUID_Word2(void)
{
return (uint32_t)(READ_REG(*((uint32_t *)(UID_BASE_ADDRESS + 8U))));
}
2019-12-23 9:39 AM
No, those relate to the type/step of IC you have ie H743 Step V
The Unique is pulled as 3x 32-bit values from memory
#define UID_BASE (0x1FFF7590UL) /*!< Unique device ID register base address */
/**
* @brief Get Word0 of the unique device identifier (UID based on 96 bits)
* @retval UID[31:0]: X and Y coordinates on the wafer expressed in BCD format
*/
__STATIC_INLINE uint32_t LL_GetUID_Word0(void)
{
return (uint32_t)(READ_REG(*((uint32_t *)UID_BASE_ADDRESS)));
}
/**
* @brief Get Word1 of the unique device identifier (UID based on 96 bits)
* @retval UID[63:32]: Wafer number (UID[39:32]) & LOT_NUM[23:0] (UID[63:40])
*/
__STATIC_INLINE uint32_t LL_GetUID_Word1(void)
{
return (uint32_t)(READ_REG(*((uint32_t *)(UID_BASE_ADDRESS + 4U))));
}
/**
* @brief Get Word2 of the unique device identifier (UID based on 96 bits)
* @retval UID[95:64]: Lot number (ASCII encoded) - LOT_NUM[55:24]
*/
__STATIC_INLINE uint32_t LL_GetUID_Word2(void)
{
return (uint32_t)(READ_REG(*((uint32_t *)(UID_BASE_ADDRESS + 8U))));
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.