2017-03-01 2:26 AM
Hello, I'm using a stm32F103c8, and I would like to know if I can use both Dac1 & Dac2 with two different DMA (it's for create a dtmf signal) ? Presently we have a sinus wave on Dac1 but nothing on the Dac2. SO, if we can help us. Thank you
2017-03-01 2:45 PM
I don't use 'F1xx but according to RM0008, yes:
12.3.7 DMA request
Each DAC channel has a DMA capability. Two DMA channels are used to service DAC channel DMA requests.And I see separate DMAEN1 and DMAEN2 bits in DAC_CR, and also two separate channels for DAC in the DMA chapter.
What have you done so far, what are the results and why do you believe they are not what they should be?
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.