cancel
Showing results for 
Search instead for 
Did you mean: 

Question about I2C Fast Mode (1MBit/s)

Oliver Richter
Associate
Posted on May 29, 2018 at 08:53

Dear STM Community,

we want to use I2C in Fast Mode Plus (1MBit/s) with a STM32F401xB MCU. The datasheet points out: 'The I2C bus

frequency can be increased up to 1 MHz.' What are the conditions and requirements to implement the pointed out solution? Can I update my in field MCUs with that feature?

I'm looking forward to your answer.

Kind Regards

Oliver

#stm32f401 #i2c-datasheet #i2c-setup
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee
Posted on May 29, 2018 at 11:15

Hello

oliver.richter

,

As noted in the

STM32F401

datasheet, please contact yourFAE or a local ST sales representative for more details about the complete solution related to I2C fast mode.

The I2C bus interface supports standard mode (up to 100 kHz) and fast mode (up to 400 kHz). The I2C bus frequency can be increased up to 1 MHz. For more details about the complete solution, please contact your local ST sales representative.

With Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
AvaTar
Lead
Posted on May 29, 2018 at 13:08

Can I update my in field MCUs with that feature?

This is only the (supposed) master.

For a successful application, your slave devices and the bus layout must support this clock frequency as well.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.