cancel
Showing results for 
Search instead for 
Did you mean: 

question about DAC

vicki19880929
Associate III
Posted on October 18, 2013 at 01:54

Hi all,

I have two questions about DAC configuration.

1. The below cofiguration code works for two analog outputs.  I can write my values to PA4 and PA5 by: 

        DAC_SetChannel1Data(DAC_Align_12b_R, 0x0000);  // PA4

        DAC_SetChannel2Data(DAC_Align_12b_R, 0x0000);  // PA5

But I wonder which part of the code links PA4 pin with DAC_channel1 and PA5 with DAC_channel2 together respectively?  

void AnalogOutput_Config(void)       

{

        GPIO_InitTypeDef                GPIO_InitStructure;

        DAC_InitTypeDef           DAC_InitStructure;

        /* GPIOA clock enable */

        RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

        /* DAC Periph clock enable */

        RCC_APB1PeriphClockCmd(RCC_APB1Periph_DAC, ENABLE);

        /*------------------------ GPIO configuration ------------------------*/

        /* Configure PA4 and PA5 as analog output */

        GPIO_InitStructure.GPIO_Pin =  GPIO_Pin_4 | GPIO_Pin_5;

        GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;

        GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;

        GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

        GPIO_Init(GPIOA, &GPIO_InitStructure);

        /* -------------------------- DAC_Channel2 Configuration --------------------*/

        DAC_DeInit();

        DAC_InitStructure.DAC_Trigger = DAC_Trigger_None;

        DAC_InitStructure.DAC_WaveGeneration = DAC_WaveGeneration_None;

        DAC_InitStructure.DAC_OutputBuffer = DAC_OutputBuffer_Disable;

        /*DAC Channel2 Init */

        DAC_Init(DAC_Channel_2, &DAC_InitStructure);

        /*Enable DAC Channel2 */

        DAC_Cmd(DAC_Channel_2, ENABLE);

        /* -----------------------------DAC_Channel1 Configuration ------------------------*/

        DAC_InitStructure.DAC_OutputBuffer = DAC_OutputBuffer_Disable;

        /*DAC Channel1 Init */

        DAC_Init(DAC_Channel_1, &DAC_InitStructure);

        /*Enable DAC Channel1*/

        DAC_Cmd(DAC_Channel_1, ENABLE);

        /* set default analog output as zero */

        DAC_SetChannel1Data(DAC_Align_12b_R, 0x0000);  // PA4

        DAC_SetChannel2Data(DAC_Align_12b_R, 0x0000);  // PA5

}

2. If one DAC channel can only be used by one analog output, at most I can only have two analog outputs. (There are only 2 dac channels for stm32l-discovery)  What can I do if I want to include more analog outputs? 

Thanks a lot.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on October 18, 2013 at 02:05

You have very little control, they are hard-wired analogue paths.

You'd use an external DAC, perhaps using the I2S interface, or SPI.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ray
Associate II
Posted on October 18, 2013 at 08:02

I used TLV5618A to extend DAC of STM32.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.