2017-08-04 1:08 PM
2017-08-04 1:35 PM
Looks like I may have been missing a ARPE bit in the CR1 register which enables the shadow buffer of the ARR register.
2017-08-04 1:37 PM
TIM2->ARR = clk - 1; // N-1 register
Can you do the update while paying attention to the phase? Check the elapsed time in the Update IRQ? ie >15ms step to next.
2017-08-04 1:44 PM
Hello!
The way you chose to handle the change of cycle and width is quite anorthodox.
The PWM generation is normaly handled by the hardware.
If you want to change the cycle and width you must put the new values to ARR and to CCR and wait tothe next update event of the counter to load the new values
If you dont want to wait until the next update event you have the option fto set the EGR.UG flag to trigger an imediate update with new values.
In your code every ttime you call the
startPWM_Test
is like to reinitialise the timer.It stops counting, loads the same values and again starts etc. .
If you want clean pwm pulses ,
just eliminate this code
//TIM2->CNT = 0;
if
(( TIM2->
CR1
& TIM_CR1_CEN ) == 0)
// first pass turn on timer and
cfg
, otherwise just load CCR2 and ARR to shadow registers{
TIM2->
CCER
&= ~
TIM_CCER_CC3E
;TIM2->
PSC
= 0;
// Set
prescaler
to 0, so APBCLK/1 i.e 1MHzTIM2->
CCMR1
= 0;
// No input capture
TIM2->
CCMR2
= TIM_CCMR2_OC3M_2 | TIM_CCMR2_OC3M_1 | TIM_CCMR2_OC3M_0 |TIM_CCMR2_OC3PE;
// Set OC3 to PWM
TIM2->
CCER
|=
TIM_CCER_CC3E
;// Enable the output on OC3 (CC3E = 1)e
TIM2->
CR1
|= TIM_CR1_CEN;
// Enable counter (CEN = 1)
}
and /or (it is your choice ) call
TIM2->
EGR |=0x01; //to imediately update the valuesThis solution pre includes proper initialisation
2017-08-04 2:08 PM
@ Clive
Thanks for noticing the -1.
@ Vangelis
This is demo code extracted from the main project to show the issue in a simplified manner. I was originally re-initializing the clock on each pass before I realized that those registers were shadow copied. I changed the code with the
if
(( TIM2->
CR1
& TIM_CR1_CEN ) == 0) statement so the timer is initialized only if the counter is off.2017-08-04 4:27 PM
Hi!
I was overtaken by the infinite loop and did not notice
this.:((
Rgrds
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.