2017-08-04 1:49 PM
I am having strange problem on some boards, we use stm32f107, it was developed 3 firmware, the first one to check if flash sector of application firmware need update, second one to erase flash of application firmware and read from a SD CARD bin file to write on flash, most are working accordingly, but on others when the firmware responsable for write flash get executed when I call fmount it returns fsmediaerror.
I tried format sd card on FAT16 and FAT32 the result is the same, tried change sd card same results.
I forgot that we are using pins PC10, PC11 e PC12, PA4 of SPI3.
I would be so grateful if anyone could help me.
#sd-card #stm32f017We’re moving the ST Community to a new platform to give you a better and more reliable community experience.