2023-02-15 2:44 PM
I want to use the STM32F769I-EVAL Board to monitor a CAN netork. I configured the CAN module as it has been shown in the CAN_Loopback and in the CAN_Networking example.
The Loopback Example does run on my eval-board. I take that as confirmation, that I set up the CAN module the richt way. However the loopback mode does not use the transciever chip because the TX Signal is directly send back on the RX Line. I tested all possible jumper combinations with JP14, JP18 and JP19. Has anyone suggestions how to get the transciever working?
2023-02-17 7:00 PM
if you want to use the CAN_Loopback example to use the CAN transceiver, then you need to modify the mode to
CanHandle.Init.Mode = CAN_MODE_NORMAL;
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.