2016-04-05 6:49 AM
I'm using STM32F446RE NUCLEO and I need to count the external pulse.I don't know how to configurate it to enable the counter.the value of counter is 0 whatever the input fruquency.
the following code is my configuration function.Thanks for your helping!
void TIM2_Configuration(void) { GPIO_InitTypeDef GPIO_InitStructure; TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; RCC_ClocksTypeDef RCC_ClockFreq; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOA,GPIO_PinSource0,GPIO_AF_TIM2); RCC_GetClocksFreq(&RCC_ClockFreq); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); TIM_DeInit(TIM2); TIM_TimeBaseStructure.TIM_Period = 0xFFFF; TIM_TimeBaseStructure.TIM_Prescaler = 2; TIM_TimeBaseStructure.TIM_ClockDivision = 0x0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure); // Time base configuration TIM_ETRClockMode2Config(TIM2, TIM_ExtTRGPSC_OFF, TIM_ExtTRGPolarity_NonInverted, 0); TIM_SetCounter(TIM2, 0); TIM_Cmd(TIM2, ENABLE); } #timer #stm32f42016-04-05 9:27 AM
Hi u.zhiyan,
TheTIM_Deinit() is disabling the clock of your Timer. Try to avoid it in that level and keep it on the top before enabling clock.
-Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.