2018-05-12 4:57 AM
Hello everyone,
I have used the following codes to (erase and then ) write to the flash in STM32F103RCT6, the problem is every time i call this function it writes every page only the first time. meaning when called for the second time, writing to the same page makes no effect (nothing is erased even). but when i hard reset (power Off and On) i can erase and write to that page again but only once again. please help me to understand what have I overlooked?!
this is my code:
HAL_FLASH_Unlock();
while((FLASH->SR&FLASH_SR_BSY)); FLASH->CR |= FLASH_CR_PER; //Page Erase Set FLASH->AR = Page_start_address; //Page Address FLASH->CR |= FLASH_CR_STRT; //Start Page Erase while((FLASH->SR&FLASH_SR_BSY)); FLASH->CR &= ~FLASH_CR_PER; //Page Erase Clear FLASH->CR |= FLASH_CR_PG; for(i=0; i<2048; i+=2) { while((FLASH->SR&FLASH_SR_BSY)); *(__IO uint16_t*)(Page_start_address + i) = DATA[i/2]; //FLASH_Program HalfWord } HAL_FLASH_Lock();Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.