STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Flash write command error

Posted on May 11, 2018 at 22:55Hello Guys, I am using STM32 L476RG microcontroller. I am trying to program it with ST Link V2 and ST link utility. The utility recognizes my microcontroller however when I try to drag and drop the code, I get a fail.T...

Cube32MX - input capture overflow detection.

Posted on May 18, 2017 at 22:46Hi.I'm trying to use TIM1's channel 1 as a spindle RPM input capture. ( device is STM32F103C8 )Knowing that the spindle has a single pulse per revolution and is rated from 0 to 30K rpm, the frequency domain is 0 to 500...

arnaljl by Associate III
  • 7430 Views
  • 16 replies
  • 1 kudos

Using an external signal to clear TIM counter

Posted on May 11, 2018 at 20:57I'm using TIM2 as a PWM. I have an (periodic) external signal that should reset the TIM2 counter to zero, so that the PWM is synchronized to the external signal. In a previous naive setup, I used the external signal to...

jsvirzi by Associate II
  • 4015 Views
  • 7 replies
  • 0 kudos

RTC Interrupt not accurate when place a function in

Posted on May 12, 2018 at 15:32I just used RTC interrupt to measure msec timing. and  I got some problem.when i write naive code in interrupt there is no problem. timing is correct and no delay. the sample code is belowvoid RTC_IRQHandler(void){    ...

jd kim by Associate II
  • 696 Views
  • 0 replies
  • 0 kudos

problem writing to flash for the second time

Posted on May 12, 2018 at 13:57Hello everyone,I have used the following codes to (erase and then ) write to the flash in STM32F103RCT6, the problem is every time i call this function it writes every page only the first time. meaning when called for ...

SPINFamily Evaluation Tool 3.2: serial protocol please?

Posted on May 12, 2018 at 07:00X-CUBE-SPN4brushed motors,SPINFamily Evaluation Tool 3.2at 28VDC.controlling demo from pc on virtual com port with the demo's gui.what is com serial protocol so i can drive it over the usb with my own gui?Source please...

Pulse counter 80 MHZ.

Posted on May 11, 2018 at 20:37Pulse counter 80 mhz input, on 180 MHZ stm32 F479Hello, I just need to keep count of an external clock input,  wich comes at about 80 mhz.I dont need to be interrupted or anything, just that this count be accessible at...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.