2018-11-05 5:39 AM
Hello! I use CubeMX to generate the init code for rcc whith LSE Crystal NX3215SA-32.768KHZ-EXS00A-MU00525 (32.768K,6PF), two 2.7pF capacitors and rtc module. Program goes to error handler after "if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)"-stroke. And if configure it with LSI, all works perfectly. And it works with LSE on STM32L496ZGT6U MCU(NUCLEO-L496ZG) with the same CubeMX configurations. I'm using Atollic Truestudio and there is no stm32l4re mcu. So i use stm32l4rg and configure .ld file for flash size. Am I right? What problem is here? I attached 2 projects here. LSE_NucleoL4 is working project for NUCLEO-L496ZG, RET6_1 is not-working project for STM32L496RET6.
2018-11-05 5:45 AM
Try to use a longer timeout for the LSE startup.
You can also try to change the LSE drive strength.
I don't Cube.
JW
2018-11-05 6:08 AM
But is your external clock actually starting and oscillating? Pipe it to the MCO pin (if supported) and probe it there.
2018-11-06 9:34 PM
I tried a longer startup time, but it i'snt work still. I cannot use pipe to MCO pin because it stops in the rcc initialization.
2018-11-06 9:53 PM
Your options would be to make sure it doesn't dump into an Error_Handler() or while(1) loop. Or work directly on the RCC_BDCR to enable the LSE and test it's readiness there.
2018-11-06 11:41 PM
> it stops in the rcc initialization.
Then don't use the pre-chewed "library" functions. You don't need to change any other clock to try to run the LSE.
> I tried a longer startup time, but it i'snt work still.
Quantify. Or, even better, wait infinitely for the experiment. The 32kHz oscillators may take a surprisingly long time to start up, especially on well-designed boards (this may sound surprising, but the fact is that crystal oscillators start up by picking up noise). Tens of seconds are not abnormal.
And, as I've said above, try to play with the LSE drive (see RCC_BDCR.LSEDRV, if there is such in your STM32 model).
And, of course, double-check your connections, both for correctness and also for bad solder joints.
JW
2019-01-14 11:39 PM
I had the exact same problem. The solution is to configure RCC_LSEDRIVE to be high.
If you use cubemx:
Configuration > RCC > LSE Drive Capability > LSE oscillator high drive capability
If you don't use cubemx, add these lines in main.c in SystemClock_Config() just after the variables declarations:
/**Configure LSE Drive Capability*/
HAL_PWR_EnableBkUpAccess();
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_HIGH);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.